how to set the efuse (OTP) with jtag

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to set the efuse (OTP) with jtag

1,567 次查看
nick76
Contributor I

Hello..

I would like to set efuse(OTP) with Jtag(DS-5) on the IMX6Q custom Board.

is it possible ?

If possible, let me know how to set the value..

Regards,

Nick

标签 (1)
0 项奖励
回复
2 回复数

1,334 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Seongwoong

one can try to implement attached baremetal sdk example

using jtag scripts, please use Chapter 25 Configuring the OCOTP Driver

pdf document.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,334 次查看
nick76
Contributor I

Thank you.

Our purpose is to live our custom board from SD memory.

- boot mode settings is possible,

- there are no pins (BT_CFG1_0~7, BT_CFG2_0~7,BT_CFG3_0~7, BT_CFG4_0~7) so it is impossible for boot by GPIO.

- there is no otg USB.

Aa a result, we have to live our custom board with JTAG(Dstream)

I don't have the jtag script..

would you explain to me in detail?

The attached file is ref. schematic

Regards,

Nick.

0 项奖励
回复