Hi
i want to set mii speed of fec as 1 Mhz on imx8mp.
how to i set mii speed 1 Mhz?
Right now it's 2.5 Mhz.
we are try to set using fec_main.c file but not able to set some time its very high frequncy.
here added fec mii speed snap
mii_speed = DIV_ROUND_UP(clk_get_rate(fep->clk_ipg), 5000000);
if (fep->quirks & FEC_QUIRK_ENET_MAC)
mii_speed--;
if (mii_speed > 63) {
dev_err(&pdev->dev,
"fec clock (%lu) too fast to get right mii speed\n",
clk_get_rate(fep->clk_ipg));
err = -EINVAL;
goto err_out;
}
holdtime = DIV_ROUND_UP(clk_get_rate(fep->clk_ipg), 100000000) - 1;
fep->phy_speed = mii_speed << 1 | holdtime << 8;
writel(fep->phy_speed, fep->hwp + FEC_MII_SPEED);
As per code we are below value are geting for 2.5 Mhz
mii_speed = 54
clk_get_rate(fep->clk_ipg) = 266666666
holdtime = 2
How to set 1 Mhz instead of 2.5 Mhz ?
which value i want to change ?
we are using imx8mp 5.4 kernel
解決済! 解決策の投稿を見る。
Hi Ankit
in general one can try to decrease value of parent clock using const imx8mp_enet_ref_sels[]
in clock driver
https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/clk/imx/clk-imx8mp.c?h=lf-5.10.y
However setting such low frequency seems out of ENET specification as i.MX8M Plus supports
only RMII and RGMII as described in sect.3.8.3 Ethernet controller (ENET) AC electrical specifications
i.MX 8M Plus Applications Processor Datasheet for Consumer Products
Best regards
igor
Hi Ankit
in general one can try to decrease value of parent clock using const imx8mp_enet_ref_sels[]
in clock driver
https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/clk/imx/clk-imx8mp.c?h=lf-5.10.y
However setting such low frequency seems out of ENET specification as i.MX8M Plus supports
only RMII and RGMII as described in sect.3.8.3 Ethernet controller (ENET) AC electrical specifications
i.MX 8M Plus Applications Processor Datasheet for Consumer Products
Best regards
igor