how to set mii speed in fec driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how to set mii speed in fec driver

跳至解决方案
2,079 次查看
ankitpanchal167
Contributor III

Hi 

i want to set mii speed of fec as 1 Mhz on imx8mp.

how to i set mii speed 1 Mhz? 

Right now it's 2.5 Mhz.

we are try to set using fec_main.c file but not able to set some time its very high frequncy. 

here added fec mii speed snap 

mii_speed = DIV_ROUND_UP(clk_get_rate(fep->clk_ipg), 5000000);
if (fep->quirks & FEC_QUIRK_ENET_MAC)
mii_speed--;
if (mii_speed > 63) {
dev_err(&pdev->dev,
"fec clock (%lu) too fast to get right mii speed\n",
clk_get_rate(fep->clk_ipg));
err = -EINVAL;
goto err_out;
}

holdtime = DIV_ROUND_UP(clk_get_rate(fep->clk_ipg), 100000000) - 1;

fep->phy_speed = mii_speed << 1 | holdtime << 8;

writel(fep->phy_speed, fep->hwp + FEC_MII_SPEED);

As per code we are below value are geting for 2.5 Mhz  

mii_speed = 54

clk_get_rate(fep->clk_ipg) = 266666666

holdtime = 2 

 How to set  1 Mhz  instead of 2.5 Mhz ? 

which value i want  to change ?

we are using imx8mp 5.4 kernel 

 

 

0 项奖励
回复
1 解答
2,067 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ankit

 

in general one can try to decrease value of parent clock using const imx8mp_enet_ref_sels[] 

in clock driver

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/clk/imx/clk-imx8mp.c?h=lf-5.10.y

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp.dtsi?...

However setting such low frequency seems out of ENET specification as i.MX8M Plus supports

only RMII and RGMII as described in sect.3.8.3 Ethernet controller (ENET) AC electrical specifications

i.MX 8M Plus Applications Processor Datasheet for Consumer Products

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,068 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ankit

 

in general one can try to decrease value of parent clock using const imx8mp_enet_ref_sels[] 

in clock driver

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/clk/imx/clk-imx8mp.c?h=lf-5.10.y

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm64/boot/dts/freescale/imx8mp.dtsi?...

However setting such low frequency seems out of ENET specification as i.MX8M Plus supports

only RMII and RGMII as described in sect.3.8.3 Ethernet controller (ENET) AC electrical specifications

i.MX 8M Plus Applications Processor Datasheet for Consumer Products

 

Best regards
igor

0 项奖励
回复