how to set audio path routing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to set audio path routing

Jump to solution
12,213 Views
fangmingan
Contributor I

We worked on the following platform:

Android 4.0 +kernel Linux 3.0

CPU i.mx6 solo

Codec:WM8960

The situation:

Codec has been registered

Then I tested the codec using tinyplay or OMXplayer, no voice on speaker or headphone!

 

The attached file <control.txt> showed the status got by tinymix. And <i.mx6-5.27.log> is system log file .

 

If I use tinymix to set "Headphone Playback Volume " to 100 , "Right Output Mixer PCM Playback Switch " and "Left Output Mixer PCM Playback Switch" to on, then plaly wav type musci by tinyplay or OMXplayer , I can hear voice on headphone.

 

<asound.conf> is from the dir of source code , external/fsl_imx_omx/release.

Should I modify this file to set audio path?

But I checked the system running on i.mx6 solo board, there is not <asound.conf> in  /system/etc dir.

 

Thanks in advance,

Fangming

Original Attachment has been moved to: control.txt.zip

Original Attachment has been moved to: i.mx6-5.27.log.zip

Original Attachment has been moved to: asound.conf.zip

Labels (3)
Tags (2)
0 Kudos
Reply
1 Solution
4,500 Views
saurabh206
Senior Contributor III

Hi,

you can refer following files for your requirement.

kernel_imx\arch\arm\mach-mx6\board-mx6q_sabresd.c

static struct mxc_audio_platform_data wm8962_data = {

    .ssi_num = 1,

    .src_port = 2,

    .ext_port = 3,

    .hp_gpio = SABRESD_HEADPHONE_DET,

    .hp_active_low = 1,

    .mic_gpio = SABRESD_MICROPHONE_DET,

    .mic_active_low = 1,

    .init = mxc_wm8962_init,

    .clock_enable = wm8962_clk_enable,

};


kernel_imx\sound\soc\codecs\wm8962.c

kernel_imx\sound\soc\imx\imx-wm8962.c

imx_hifi_hw_params()

imx_audmux_config().

Thanks,

Saurabh


View solution in original post

0 Kudos
Reply
4 Replies
4,500 Views
fangmingan
Contributor I

Anyone can help?

Thanks and Best Regards,

Fangming


0 Kudos
Reply
4,501 Views
saurabh206
Senior Contributor III

Hi,

you can refer following files for your requirement.

kernel_imx\arch\arm\mach-mx6\board-mx6q_sabresd.c

static struct mxc_audio_platform_data wm8962_data = {

    .ssi_num = 1,

    .src_port = 2,

    .ext_port = 3,

    .hp_gpio = SABRESD_HEADPHONE_DET,

    .hp_active_low = 1,

    .mic_gpio = SABRESD_MICROPHONE_DET,

    .mic_active_low = 1,

    .init = mxc_wm8962_init,

    .clock_enable = wm8962_clk_enable,

};


kernel_imx\sound\soc\codecs\wm8962.c

kernel_imx\sound\soc\imx\imx-wm8962.c

imx_hifi_hw_params()

imx_audmux_config().

Thanks,

Saurabh


0 Kudos
Reply
4,500 Views
fangmingan
Contributor I

Dear Saurabh,

Thank you for your attention!

Yes, We mainly modified these 3 files you mentioned. And I think the audio card has been registered successfully.

You can find the following information on log file

ALSA device list:

  #0: wm8960-audio

In the  file kernel_imx\sound\soc\imx\imx-wm8960.c, we changed widget and audio_map

/* imx card dapm widgets */

static const struct snd_soc_dapm_widget imx_dapm_widgets[] = {

        SND_SOC_DAPM_HP("Headphone Jack", NULL),

        SND_SOC_DAPM_SPK("Ext Spk_L", NULL),

        SND_SOC_DAPM_SPK("Ext Spk_R", NULL),

        SND_SOC_DAPM_MIC("AuxMIC", NULL),

        SND_SOC_DAPM_MIC("MainMIC", NULL),

};

static const struct snd_soc_dapm_route audio_map[] = {

        { "Headphone Jack", NULL, "HP_L" },

        { "Headphone Jack", NULL, "HP_R" },

        { "Ext Spk_L", NULL, "SPK_LP" },

        { "Ext Spk_L", NULL, "SPK_LN" },

        { "Ext Spk_R", NULL, "SPK_RP" },

        { "Ext Spk_R", NULL, "SPK_RN" },

        { "MICB", NULL, "MainMIC" },

        { "LINPUT1", NULL, "MICB" },

        { "MICB", NULL, "AuxMIC" },

        { "LINPUT2", NULL, "MICB" },

};

Then  in funtion imx_wm8960_init, enable  speaker and main mic

static int imx_wm8960_init(struct snd_soc_pcm_runtime *rtd)

{

.....

snd_soc_dapm_enable_pin(&codec->dapm, "Ext Spk_L");

snd_soc_dapm_enable_pin(&codec->dapm, "Ext Spk_R");

snd_soc_dapm_enable_pin(&codec->dapm, "MainMIC");


......

}

But  when playing whether by tinyplay or OMXPlayer, I need to mix the path by tinymix!

Why?



0 Kudos
Reply
4,500 Views
gavinbao
Contributor I

can you share you source.my code can playback ,but not capture.thanks

0 Kudos
Reply