how to read/write uart 2/3/4 on u-boot with imx8mn ddr3l evk board ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to read/write uart 2/3/4 on u-boot with imx8mn ddr3l evk board ?

1,184 Views
justin-inno
Contributor I

Hi All.

I am working on  imx8mn ddr3l system and changed console port with uart1 from default 2 
 

see to check  [imx8mn ddr3l evk] how to setup console port uart1 frm default uart2 - NXP Community

Now I am trying to read/write uart 2/3/4 on u-boot.

But I don't have idea how to read/write uart port on u-boot.
here is my trying example.
========================================================

#include <common.h>
#include <command.h>
#include <dm.h>
#include <serial.h>

#define UART_TIMEOUT_MS 10000

static int do_uart_test(struct cmd_tbl *cmdtp, int flag, int argc, char *const argv[])
{
const char *message;
const char *uart_base_str;
ulong uart_base;

if (argc != 3) {
printf("Usage: uart_test <uart_base> <message>\n");
return CMD_RET_USAGE;
}

/* UART base address */
uart_base_str = argv[1];
message = argv[2];
uart_base = simple_strtoul(uart_base_str, NULL, 16);

/* UART base address */
printf("Setting UART base address to 0x%lx\n", uart_base);
serial_setbrg(); // UART

printf("Sending message to UART at base address 0x%lx: %s\n", uart_base, message);

for (const char *p = message; *p; p++) {
serial_putc(*p);
}

serial_putc('\n');
printf("Message sent successfully.\n");

printf("Receiving data:\n");
ulong start_time = get_timer(0);
while (1) {
if (serial_tstc()) { // check if received data exist
char c = serial_getc();
if (c == '~') { // setup for exit condition with ~
break;
}
putc(c); // show received character
start_time = get_timer(0);
}
if (get_timer(start_time) > UART_TIMEOUT_MS) {
printf("\nTimeout: No data received for %d ms\n", UART_TIMEOUT_MS);
break;
}
}

printf("\nReception finished.\n");
return CMD_RET_SUCCESS;
}
U_BOOT_CMD(
uart_test, 3, 1, do_uart_test,
"Test UART communication ",
"<uart_base> <message>\n"
" - Send <message> to the specified UART at <uart_base>.\n"
" - Terminate reception on '~'."
);

========================================================

Let me know how to read/write uart on u-boot ?

-Best Regards-

0 Kudos
Reply
4 Replies

1,057 Views
justin-inno
Contributor I

HI.. it works now,
I got a useful link about the issue.  Re: how to read/write uart 2/3/4 on u-boot with imx8mn ddr3l evk board ? - NXP Community
Now, I can tx via uart2.

0 Kudos
Reply

1,164 Views
Chavira
NXP TechSupport
NXP TechSupport

HI @justin-inno!

Unfortunately we don't have examples reading UART from U-boot.

I recommend to consult the U-Boot Documentation for that.

 

Best Regards!

Chavira

0 Kudos
Reply

1,106 Views
justin-inno
Contributor I
thanks for your rely,

There is no idea to get way for uart tx/rx.

I am trying to get way to tx/rx UART.
if you have any idea later, let me know it...
0 Kudos
Reply

1,091 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @justin-inno!

You can develop a program to run in u-boot, maybe you can develop your own driver.

0 Kudos
Reply