how to power up i.mx sololite

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to power up i.mx sololite

1,499件の閲覧回数
thangameenaraje
Contributor II

what will happen if i given a power supply without sd card.. it will display anything?

0 件の賞賛
返信
4 返答(返信)

1,426件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi THANGAMEENA

if any boot mode fails, processor will go to to Serial Downloader mode

described in sect.8.2.4 Serial Downloader IMX6SLRM

or try recovery mode described in sect.8.9 Recovery Devices:

The Chip supports recovery devices. If primary boot device fails, boot ROM

will try to boot from recovery device using one of I2C or ECSPI ports.

For enabling recovery device BOOT_CFG4[6] fuse must be set.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,426件の閲覧回数
sangilikumar
Contributor I

now i am preparing my sd card.. i run the script.. fsl-sdcard-partition.sh.. it will created four partition only

data

system // mysystem.img is 700 mb but it created only 450 mb .. unable to copy

cache

vendor

but we need boot and recovery partition too to put boot.img and recovery.img

how to flash sd card.

0 件の賞賛
返信

1,426件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi THANGAMEENA

for flashing problems please create new thread.

~igor

0 件の賞賛
返信

1,426件の閲覧回数
saurabh206
Senior Contributor III

Hi,

It depends upon your boot mode settings?

0 件の賞賛
返信