how to make secure boot of kernel and RFS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how to make secure boot of kernel and RFS

跳至解决方案
1,860 次查看
PramodKumar
Contributor IV

Hi,

Please help us to make encrypted kernel and RFS and boot the i.MX233 based board.

Regards,

Pramod Kumar

标记 (6)
0 项奖励
回复
1 解答
1,584 次查看
Yuri
NXP Employee
NXP Employee

   The i.MX23 supports encrypted boot, described in section  5.1 (i.MX28 encrypted boot in a nut-shell)
of the app note AN4555 (Secure Boot with i.MX28 HAB Version 4). Also please refer to Chapter 35

(Boot Modes) of the i.MX23 Reference Manual. Note, the i.MX23 does not support HAB technology.

  So, it is possible to use encrypted boot of a bootloader ( say, U-boot) and further activities regarding
kernel and RFS should be performed by U-boot. Sorry, we do not have an app note about this.

Regards,

Yuri.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,585 次查看
Yuri
NXP Employee
NXP Employee

   The i.MX23 supports encrypted boot, described in section  5.1 (i.MX28 encrypted boot in a nut-shell)
of the app note AN4555 (Secure Boot with i.MX28 HAB Version 4). Also please refer to Chapter 35

(Boot Modes) of the i.MX23 Reference Manual. Note, the i.MX23 does not support HAB technology.

  So, it is possible to use encrypted boot of a bootloader ( say, U-boot) and further activities regarding
kernel and RFS should be performed by U-boot. Sorry, we do not have an app note about this.

Regards,

Yuri.

0 项奖励
回复