how to make a 4.x rootfs for imx53QSB

cancel
Showing results for 
Search instead for 
Did you mean: 

how to make a 4.x rootfs for imx53QSB

479 Views
wenmingfeng
Contributor III

Hello,

I see some people get imx53QSB support kernel 4.4.x and ubuntu16.04.1, I tried with my imx535QSB and make it boot up.

Almost every thing works except the snd card.

My question is: Does somebody try to use desktop rootfs on imx53 serial, or have a way to build new rootfs with kernel 4.x?

thanks!

Wenming 

Labels (4)
0 Kudos
2 Replies

345 Views
wenmingfeng
Contributor III

Hi igor,

Thanks for your reply. Yes  the document helpful but linux-2.6-imx-rel_imx_3.14.52_1.1.0_ga this one used kernel 2.6.x or it is 3.14.x?

Regards!

Wenming

0 Kudos

345 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wenming 

one can check below guidleines, seems it may work for i.MX53 too

Installing Ubuntu Rootfs on NXP i.MX6 boards | NXP Community 

For imx53QSB problems with kernel 4.4.x one can post on kernel mail list.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos