how to load freescale nand driver in WEC 7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to load freescale nand driver in WEC 7

Jump to solution
1,413 Views
alexeym
Contributor III

Hello all!

I've got custom hardware based on mx53qsb.

I've modified necessary pieces of code. But can't get nand work.

I've placed some keys to registry:

[HKEY_LOCAL_MACHINE\System\StorageManager\AutoLoad\FlashPDD]

    "DriverPath"="Drivers\\BuiltIn\\FlashPDD"

    "LoadFlags"="dword:2"

    "BootPhase"="2"

    "Order"="0"

[HKEY_LOCAL_MACHINE\Drivers\BuiltIn\FlashPDD]

    "Dll"="flashmdd.dll"

    "FlashPddDll"="flashpdd_nand.dll"

    "Prefix"="DSK"

    "Profile"="MSFlash"

    "IClass"=multi_sz:"{A4E7EDDA-E575-4252-9D6B-4195D48BB865}",

                     "{8DD679CE-8AB4-43c8-A14A-EA4963FAA715}"

    "FriendlyName"="NAND Flash Driver"

    "Order"=dword:20

    "Priority256"=dword:76

; @CESYSGEN IF FILESYS_FSREGHIVE

    ;"Flags"=dword:1000

; @CESYSGEN ENDIF FILESYS_FSREGHIVE

[HKEY_LOCAL_MACHINE\System\StorageManager\Profiles\MSFlash]

    "DefaultFileSystem"="FATFS"  

    "PartitionDriver"="FLASHPART.dll"

    "AutoFormat"=dword:1

    "AutoPart"=dword:1

    "AutoMount"=dword:1

    "Name"="NAND FLASH Storage"

    "Folder"="NANDFlash"

    ;"FormatExfat"=dword:1

; @CESYSGEN IF FILESYS_FSREGHIVE

    "FormatTfat"=dword:1

    ;"MountAsBootable"=dword:1

    ;"MountPermanent"=dword:1

; @CESYSGEN ENDIF FILESYS_FSREGHIVE  

Labels (2)
0 Kudos
Reply
1 Solution
1,203 Views
alexeym
Contributor III
0 Kudos
Reply
1 Reply
1,204 Views
alexeym
Contributor III

Found answer here.

0 Kudos
Reply