HP-xw4400-Workstation:~/Desktop/L3.0.35_4.1.0_130816_source/ltid/ltib$ ./ltib
defined(@array) is deprecated at /home/cyient/Desktop/L3.0.35_4.1.0_130816_source/ltid/ltib/bin/Ltibutils.pm line 362.
(Maybe you should just omit the defined()?)
ltib cannot be run because one or more of the host packages needed to run it
are either missing or out of date or not in ltib's standard path. Please
install/upgrade these packages on your host. If you have your own utilities
in non-standard paths, please add an entry into the .ltibrc file for example:
%path_std
/usr/local/bin:/usr/bin:/bin:/usr/bin/X11:/usr/X11R6/bin:/my/own/exes
Package Minimum ver Installed info
------- ----------- ---------------
zlib 0 not installed
Died at ./ltib line 1409.
traceback:
main::host_checks:1409
main:554
Started: Tue Jan 20 11:45:13 2015
Ended: Tue Jan 20 11:45:15 2015
Elapsed: 2 seconds
Build Failed
Exiting on error or interrupt
Hi Viswanath
first please install packages as suggests attached document.
Also, for example, various Ubuntu distributions can move libs to different locations,
so ltib fails find them. Below links may be helpful.
i.MX Linux BSP Environment Setup
https://community.freescale.com/docs/DOC-93454
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
OK and I am installing the list of paclages now. and i am following this link : https://community.freescale.com/docs/DOC-100725
before this i got "zlib not installed" and the build was failed.
defined(@array) is deprecated at /home/cyient/Desktop/L3.0.35_4.1.0_130816_source/ltid/ltib/bin/Ltibutils.pm line 362.
(Maybe you should just omit the defined()?)
ltib cannot be run because one or more of the host packages needed to run it are either missing or out of date or not in ltib's standard path. Please install/upgrade these packages on your host. If you have your own utilities
in non-standard paths, please add an entry into the .ltibrc file for example:
%path_std
/usr/local/bin:/usr/bin:/bin:/usr/bin/X11:/usr/X11R6/bin:/my/own/exes
Package Minimum ver Installed info
I installed all the packs and tools and also applied the patch for 14.04 ubuntu also but i got an build faild.
can you please help in this:
cyient@cyient-HP-xw4400-Workstation:~/Desktop/L3.0.35_4.1.0_130816_source/ltib/ltib$ ./ltib
I ran the command: sudo -S -l which returned:
Matching Defaults entries for cyient on cyient-HP-xw4400-Workstation:
env_reset, mail_badpass, secure_path=/usr/local/sbin\:/usr/local/bin\:/usr/sbin\:/usr/bin\:/sbin\:/bin
User cyient may run the following commands on cyient-HP-xw4400-Workstation:
(ALL : ALL) ALL
This means you don't have sudo permission to execute rpm commands as root
without a password. This is needed for this build script to operate correctly.
To configure this, as root using the command "/usr/sbin/visudo",
and add the following line in the User privilege section:
cyient ALL = NOPASSWD: /usr/bin/rpm, /opt/freescale/ltib/usr/bin/rpm
traceback:
main::check_sudo_setup:2467
main::host_checks:1413
main:554
Started: Tue Jan 20 14:44:27 2015
Ended: Tue Jan 20 14:44:27 2015
Elapsed: 0 seconds
Build Failed
Exiting on error or interrupt
cyient@cyient-HP-xw4400-Workstation:~/Desktop/L3.0.35_4.1.0_130816_source/ltib/ltib$
regards,
Viswanath K
for "sudo permission" please look at
http://cache.freescale.com/files/dsp/doc/app_note/AN3875.pdf p.44