Hello ALL,
I need to interface the 3.2" st7789s Lcd as RGB565 parallel and initialize with SPI, i configured the lcd data pins as per Board (SABRE-2|Automotive-Infotainment|i.MX6|NXP ) and i also attached the both data sheet of lcd and Schematic of board, i am struggling to initialize with SPI driver in linux imx6 3.10 version, can you please anyone help me to come out this problem,
Thanks in advance,
Best Regards
nandishsg
Hi Nandish,
if the ST7789S is not in Linux as a display driver, then you need to add it by yourself. We use the following display module for i.MX boards, it's the same principle. RGB + init interface like I2C or SPI. Maybe you can use the existing implementation as a basis for your own implementation:
https://www.element14.com/community/docs/DOC-68483/l/43-lcd-module-and-adapter-board
Look into the "Documents" and "Download" section.
In following link you find a code snippet which shows the SPI commands for the ST7789: http://www.newhavendisplay.com/app_notes/2-4TFT_ST7789.txt
Data sheet of the ST7789S can be found here: http://www.hpinfotech.ro/ST7789S.pdf
It is also very similar to the display driver ILI9341 (see here 320x240 controller differences ST7789S and ILI9341 [Solved] | AVR Freaks), so overall it shouldn't be a problem to get this done. Except if you don't know how to patch this into Linux :smileycool:
But if you are successful somehow, don't hesitate to post your success story here!
Regards,
Bernhard.
Thank you Bernhand Fink,
Hi nandishsg
NXP has special service for helping with porting custom
drivers Professional Services:
http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE
Best regards
igor
Thank You Igorpadykov,