how to increase DDR clock in i.mx6 dual lite

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to increase DDR clock in i.mx6 dual lite

2,050件の閲覧回数
saida
Contributor II

Hi

My ddr3 is working at 400mhz

can i increase it to 800mhz, if possible what is the procedure ?

thanks and regards

saida

ラベル(1)
タグ(1)
5 返答(返信)

1,864件の閲覧回数
saida
Contributor II

Hi jan spurek

Thank you

0 件の賞賛
返信

1,864件の閲覧回数
saida
Contributor II

hi

i have a custom made board based on i.mx6 with 2gb ddr

i have set 2gb  configuration in u-boot

but u-boot is recognizing it 1gb only

what could be the problem

regards

sadia

0 件の賞賛
返信

1,864件の閲覧回数
jan_spurek
NXP Employee
NXP Employee

Hello Saida,

you need to input your new configuration in the Script Aid spreadsheet and change the affected registers in DCD accordingly.

Best Regards,

Jan

1,864件の閲覧回数
saida
Contributor II

ok

i will try it and come back to you

thank you

regards saida

0 件の賞賛
返信

1,864件の閲覧回数
jan_spurek
NXP Employee
NXP Employee

Hello Saida,

400 MHz is the maximal supported frequency for i.MX6DL.

Best Regards,

Jan