how to increase DDR clock in i.mx6 dual lite

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to increase DDR clock in i.mx6 dual lite

966 次查看
saida
Contributor II

Hi

My ddr3 is working at 400mhz

can i increase it to 800mhz, if possible what is the procedure ?

thanks and regards

saida

标签 (1)
标记 (1)
5 回复数

780 次查看
saida
Contributor II

Hi jan spurek

Thank you

0 项奖励

780 次查看
saida
Contributor II

hi

i have a custom made board based on i.mx6 with 2gb ddr

i have set 2gb  configuration in u-boot

but u-boot is recognizing it 1gb only

what could be the problem

regards

sadia

0 项奖励

780 次查看
jan_spurek
NXP Employee
NXP Employee

Hello Saida,

you need to input your new configuration in the Script Aid spreadsheet and change the affected registers in DCD accordingly.

Best Regards,

Jan

780 次查看
saida
Contributor II

ok

i will try it and come back to you

thank you

regards saida

0 项奖励

780 次查看
jan_spurek
NXP Employee
NXP Employee

Hello Saida,

400 MHz is the maximal supported frequency for i.MX6DL.

Best Regards,

Jan