how to increase DDR clock in i.mx6 dual lite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to increase DDR clock in i.mx6 dual lite

1,920 Views
saida
Contributor II

Hi

My ddr3 is working at 400mhz

can i increase it to 800mhz, if possible what is the procedure ?

thanks and regards

saida

Labels (1)
Tags (1)
5 Replies

1,734 Views
saida
Contributor II

Hi jan spurek

Thank you

0 Kudos
Reply

1,734 Views
saida
Contributor II

hi

i have a custom made board based on i.mx6 with 2gb ddr

i have set 2gb  configuration in u-boot

but u-boot is recognizing it 1gb only

what could be the problem

regards

sadia

0 Kudos
Reply

1,734 Views
jan_spurek
NXP Employee
NXP Employee

Hello Saida,

you need to input your new configuration in the Script Aid spreadsheet and change the affected registers in DCD accordingly.

Best Regards,

Jan

1,734 Views
saida
Contributor II

ok

i will try it and come back to you

thank you

regards saida

0 Kudos
Reply

1,734 Views
jan_spurek
NXP Employee
NXP Employee

Hello Saida,

400 MHz is the maximal supported frequency for i.MX6DL.

Best Regards,

Jan