how to give time critical signals like clock to sensors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to give time critical signals like clock to sensors

1,497 Views
sribinkr
Contributor I

I want to give 800khz clock to sensor through i.MX6q sabre lite board.Currently I am using Yocto dora as OS.Pls give suggestions

Labels (2)
Tags (1)
0 Kudos
Reply
3 Replies

1,430 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

What kind of sensor you are working with? Many of them are interfaced via a serial protocol like I2C or SPI. The iMX6Q features different modules that can help to achieve what you need. It woulb nice to get more information about the sensor you want to use.

Best Regards,

Alejandro

0 Kudos
Reply

1,430 Views
gary_bisson
Senior Contributor III

Hi Alejandro,

This post is a duplicate of the following:

time critical signals to sensors through i.mx6 q sabre lite board

Please close.

Regards,

Gary

0 Kudos
Reply

1,430 Views
alejandrolozan1
NXP Employee
NXP Employee

Thank Gary!

Regards,

Alejandro

0 Kudos
Reply