Hi,
We have got the I.MX6 reference board (Wandboard Quad). Serial port of this board is connected to Host PC which is running with Ubuntu and minicom. When we are powering the board, we are getting the messages. when it is asking for "Hit any key to stop autoboot" we are pressing spacebar/ESC. then it is stopping at =>. How to get the U-Boot shell (U-Boot>)
Please find the output of the minicom window as follows:
U-Boot 2014.04 (Jun 01 2014 - 21:28:55) armhf.com
CPU: Freescale i.MX6Q rev1.2 at 792 MHz
Reset cause: POR
Board: Wandboard
DRAM: 2 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
*** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
Net: FEC [PRIME]
Hit any key to stop autoboot: 0
=>
 
					
				
		
Hi,
"=>" is the boot shell. You can see the boot script (u-boot environmental variables) by "printenv" command. To change a variable or to a new one use the "setenv" command. If you enter the "saveenv" command, then only your environmental variable saved on to your SD card, if the environment you added is only for testing or for one time boot, do not run the "saveenv" command. Running "run bootcmd" will load your kernel, dtb etc if you stop normal boot.
 
					
				
		
 jan_spurek
		
			jan_spurek
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		The "=>" signalls, that you are in the U-Boot shell. It is the default prompt string. To change the prompt string, you must modify the CONFIG_SYS_PROMPT parameter and recompile.
 
					
				
		
 jian_jiang
		
			jian_jiang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
It is the U-Boot shell.
E.g. you can input the following two commands to set the boot delay time to 5s.
=> setenv bootdelay 5
=> saveenv
All the best
Jian Jiang
-----------------------------------------------------------------------------------------------------------------------
PS: If my comment answers your question, please click Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------