Hello,
I'm working with a sensor that outputs a RAW10 (0x2B) image plus Embedded Data (MetaData) (0x12) as shown in the image,But I can't get RAW10 data and MetaData.

I just want to receive the RAW10 data, metaData is irrelevant.
And I found this thread https://community.nxp.com/t5/i-MX-Processors/Does-iMX8M-CSI-support-metadata-embedded-data/m-p/97754...
I set CSI to receive generic data, But I still can't get any data.
Below are som register data.
MIPI_CSI_PHY_STATE : value=0x00000300
MIPI_CSI_DATA_IDS_1 : value=0x00000000
MIPI_CSI_DATA_IDS_2 : value=0x00000000
MIPI_CSI_ERR1 : value=0x10000110
MIPI_CSI_ERR2 : value=0x00000100
IPU1_CSI1_SENS_CONF : value=0x04009B00
So what shall i do, please tell me.
Thanks.
@jamesbone