how to flash custom scfw image in IMX8QXP using JTAG ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to flash custom scfw image in IMX8QXP using JTAG ?

1,080 次查看
krunaldhonde
Contributor I

 

We are having custom board similar to IMX8QXP in which we are not having usb type c and SD card slot.

We want to flash custom scfw image into board using JTAG. We have used following link to generate scfw image. Does this link is correct ?

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Getting-s...

How to flash generated SCFW image using JTAG ?

0 项奖励
回复
1 回复

1,068 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Krunal

 

>We have used following link to generate scfw image. Does this link is correct ?

 

yes

 

>How to flash generated SCFW image using JTAG ?

 

I am afraid it is not possible. For for writing flash.bin (SCFW image) to SD one can
follow sect.6.1 Run an example application on the M4 core Getting Started with MCUXpresso

SDK for MEK-MIMX8QX.pdf included in SDK_MEK-MIMX8QX package available on  https://mcuxpresso.nxp.com/en/welcome

 

Best regards
igor