Hi,
is there way to find iMX8QXP Silicon revision A0 / B0? please let us know.
Will boot loader start address (SD card Flashing address) depends on Silicon revision? please provide details on this.
Thanks in advance
Poons.
解決済! 解決策の投稿を見る。
Hello,
You may identify the silicon revision by the marking if it ends in A correspond to rev A0, same goes for B and C revisions.
MiMX8QX6AVLFZAB indicates that it is an i.MX 8X B0 part
Regarding uboot offset you're correct, if the full SD/eMMC card image (.sdcard/.wic) is not used and copying the bootloader manually the offset for A0 revision is 33 while for B0 is 32
i.e. copying a i.MX 8X B0 part bootloader image
$ sudo dd if=<u-boot image> of=/dev/sdx bs=1k seek=32 conv=fsync
Best regards,
Aldo.
Hello,
You may identify the silicon revision by the marking if it ends in A correspond to rev A0, same goes for B and C revisions.
MiMX8QX6AVLFZAB indicates that it is an i.MX 8X B0 part
Regarding uboot offset you're correct, if the full SD/eMMC card image (.sdcard/.wic) is not used and copying the bootloader manually the offset for A0 revision is 33 while for B0 is 32
i.e. copying a i.MX 8X B0 part bootloader image
$ sudo dd if=<u-boot image> of=/dev/sdx bs=1k seek=32 conv=fsync
Best regards,
Aldo.
Sorry for reopening this, but Is there a way we can recover a board after flashing a bad image revision? We already attempted to use uuu and flash the correct one but it complains about [LIBUSB_ERROR_IO] SDPS: boot .bin-flash
Hello @mikeMJD,
Please do help me by creating a new community thread so it may be easier to follow-up on your issue.
Anyway, taking a quick look I see that there is an space beetween boot and .bin if this is the case on the UUU command you have used, it may lead to issues when attempting to flash.
Regards,
Aldo.