how to enable mipi display in u-boot for i.mx8mq

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to enable mipi display in u-boot for i.mx8mq

ソリューションへジャンプ
1,780件の閲覧回数
kimjaeseol
Contributor I

I'm developping some embeded board with i.MX8mq

I want to know how to apply it.

If you have a patch, please let me know.

thank you.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,656件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Probably it could be possible, but I cannot guarantee anything. I can see that the dts from u-boot, has support for the MIPI-DSI. However, the only driver that I could find is for HDMI. Probably you will need to add the MIPI driver to u-boot. Unfortunately, I can not tell you if this the only thing that you need. This is as far as I can go. I apologize for the inconveniences this could give you.

Best Regards,

Diego.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,657件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Probably it could be possible, but I cannot guarantee anything. I can see that the dts from u-boot, has support for the MIPI-DSI. However, the only driver that I could find is for HDMI. Probably you will need to add the MIPI driver to u-boot. Unfortunately, I can not tell you if this the only thing that you need. This is as far as I can go. I apologize for the inconveniences this could give you.

Best Regards,

Diego.

0 件の賞賛
返信
1,656件の閲覧回数
kimjaeseol
Contributor I

Hi diego.

Thank you for your reply.

0 件の賞賛
返信