how to enable mipi display in u-boot for i.mx8mq

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to enable mipi display in u-boot for i.mx8mq

Jump to solution
1,735 Views
kimjaeseol
Contributor I

I'm developping some embeded board with i.MX8mq

I want to know how to apply it.

If you have a patch, please let me know.

thank you.

Labels (1)
0 Kudos
Reply
1 Solution
1,611 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Probably it could be possible, but I cannot guarantee anything. I can see that the dts from u-boot, has support for the MIPI-DSI. However, the only driver that I could find is for HDMI. Probably you will need to add the MIPI driver to u-boot. Unfortunately, I can not tell you if this the only thing that you need. This is as far as I can go. I apologize for the inconveniences this could give you.

Best Regards,

Diego.

View solution in original post

0 Kudos
Reply
2 Replies
1,612 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Probably it could be possible, but I cannot guarantee anything. I can see that the dts from u-boot, has support for the MIPI-DSI. However, the only driver that I could find is for HDMI. Probably you will need to add the MIPI driver to u-boot. Unfortunately, I can not tell you if this the only thing that you need. This is as far as I can go. I apologize for the inconveniences this could give you.

Best Regards,

Diego.

0 Kudos
Reply
1,611 Views
kimjaeseol
Contributor I

Hi diego.

Thank you for your reply.

0 Kudos
Reply