There are three MICs on our mx6q board with wm8962, and the hardware connection is:
IN2L <---> main mic 1
IN3R <---> headset mic
IN4R <---> main mic2
How to enable main mic1/2, anybody have any ideas?
Thanks!
Solved! Go to Solution.
jackmao Aug 19, 2013 8:18 PM (in response to imxcommunityscout)
Hi,
what's your meaning to enable MIC, the mic process the analog signal, it's always powered up, if you want to record may enable the conduction to the input signal
best regards
Jack
jackmao Aug 19, 2013 8:18 PM (in response to imxcommunityscout)
Hi,
what's your meaning to enable MIC, the mic process the analog signal, it's always powered up, if you want to record may enable the conduction to the input signal
best regards
Jack
hi,Karina,
I want to use two mic on our imx6q board with wm8962 ,hardware connection is :
IN3R <---> main mic 1
IN4L <---> main mic2
I use the android system,and the main mic 1 is OK,I can use it to talk. But the main mic2 is not OK .
where i must to modify the BSP code ?
Plese give me some advise
thanks