how to enable linux suspend to disk or MMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to enable linux suspend to disk or MMC

1,958 Views
sunyd
Contributor I

hi,

pastedImage_1.png

because need implement Low  power  consumption,and suspend to RAM unable tomeet needs,and suspend to disk or MMC should  be,but how do i configure linux kernel  to implement the feature 

thank you!!!

Labels (1)
0 Kudos
Reply
1 Reply

1,796 Views
igorpadykov
NXP Employee
NXP Employee

Hi sunyd

unfortunately it is not supported in nxp bsps, one can try to implement

it using suggestions on:

Suspend To Disk For ARM - eLinux.org 

https://community.nxp.com/docs/DOC-99733 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply