how to do with NVCC_LVDS2P5 pin?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to do with NVCC_LVDS2P5 pin?

992 Views
翔李
Contributor IV

HI,

Now,I do not connect pin NVCC_LVDS2P5 to VDDHIGH_CAP2.5V OF IMX6D,the pin on the PCB board is connect nothing but NULL,I am going to find a way to power the pin,but it is impossible to connect a fly wire to the pin under the BGA.

Is there other way to power NVCC_LVDS2P5 pin? Do it need to power it to boot the IMX6D?

thanks.

0 Kudos
Reply
1 Reply

894 Views
art
NXP Employee
NXP Employee

Q. Is there other way to power NVCC_LVDS2P5 pin?

A. No, there is no way to power the NVCC_LVDS2P5 pin other than to externally connect it to 2.5V supply.

Q. Do it need to power it to boot the IMX6D?

A. Yes, this is mandatory to power the NVCC_LVDS2P5 pin since the NVCC_LVDS2P5 power rail supplies a part of the DDR3 PHY circuit.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply