how to disable or remove the unwanted modules in kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to disable or remove the unwanted modules in kernel

935 Views
srinivas_123
Contributor III

I am using a customized IMX8M Plus board and have built the "IMXLXYOCTOUG v.LF6.6.3_1.0.0" BSP using Yocto.

For kernel customization, I need to remove or disable unwanted modules in the kernel.

I don't know how to disable or remove kernel modules. If anyone knows, please help me.

I know a little bit about disabling nodes in the DTS file, but I'm not sure if I can change the imx_v8_defconfig file. Will this help reduce the boot time or not?

Thanks and Regards

Srinivas

0 Kudos
Reply
1 Reply

905 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @srinivas_123 

I hope you are doing well.

 

I believe the AN14093 can helps to you in this request. Please refer to the chapter 8.2 Remove the unnecessary drivers and file systems.

Also, there is explained how to measure the boot time and how to do a lot of optimizations from Bootloader and kernel.

 

Best regards,

Salas.

0 Kudos
Reply