how to copy to flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to copy to flash

1,788 Views
saida
Contributor II

hi  i.mx6 community

i have i.mx6 dl sabre board with this reference i made custom board and i am ready to port u-boot which is sabre board's u-boot

can i load u-boot.imx to RAM than copy to NOR FLASH (s29jl064h chip).

how to do this ?

can any one help in this regard

can a

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

1,660 Views
Yuri
NXP Employee
NXP Employee

  Please use the enclosed MFG configuration as an example.

It loads U-boot to i.MX6 DRAM. Than You may use NFS, TFTP,

FAT SD to load and burn any image, assuming U-boot has the

needed drivers.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,659 Views
saurabh206
Senior Contributor III

Hi Saida

You can use MFG Tool provided by Freescale. It has support to update firmware on NOR FLASH.

Thanks

Saurabh

0 Kudos
Reply

1,660 Views
saida
Contributor II

hi thanks for your reply

can you send any doc or pdf which gives procedure for this

this is my new board i am going to use arm ds5

i am following this procedure

1. load u-boot using arm ds-5 and run from ram

2.load u-boot.imx binary in to ram in another location than i will use cp command to write into nor flash

is this works ?

thanks

0 Kudos
Reply

1,660 Views
Yuri
NXP Employee
NXP Employee

Saida, hi !

  You may create SR via FSL Web in order to get some recommendations about U-boot

debugging with DS-5.

Regards,

Yuri.

0 Kudos
Reply