I bought MCIMX6QP-SDB recently.
I am trying to connect USB CMOS Camera(logitech C920) to USB OTG port on MCIMX6QP-SDB.
I used the following BSP(u-boot-2018-03, linux-imx-4.9.88).
repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.98-2.0.0_ga.xml
I configured linux kernel config file to include USB VIDEO CLASS driver into kernel.
I selected the following items using "make menuconfig"
Device Drivers -> Multimedia support -> Media USB Adapters
<*> USB Video Class (UVC)
[*] UVC input events device support
<*> GSPCA based webcams
It didn't even detect usb device when I connected usb camera to USB OTG.
I think detection usb camera is the first step to use it.
uvcvideo and ehci drivers are included in linux kernel.
I am not sure USB OTG port on MCIMX6QP-SDB supports the usb host.
Can I get any advice to use usb camera with MCIMX6QP-SDB?