how to connect optical SFP module to imx28 MCU?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to connect optical SFP module to imx28 MCU?

7,123 次查看
Radist
Contributor II

Hello gentleman, does anybody know how to connect optical SFP module (125MBit) to imx287 MCU with MII MAC? i found, that standard PHY LAN8720 can't be used for that, so looks like i need special PHY. There are not so many information about it in the google at all...

Thanks for any info,

Regards, Sergii

标签 (1)
标记 (3)
4 回复数

4,967 次查看
Yuri
NXP Employee
NXP Employee

  As known Ethernet is supported under different media, in particular

there is Fiber Interface in 100BASE-FX.

Please look at section 5.2.1.2 (Fiber Interface) of classical transceiver LXT971A.

< http://cortina-systems.com/products/download/398 >

General information may be found here :

< http://cortina-systems.com/products/download/165 >

  So, two solutions may be considered when using i.MX28 ENET with optic media :

1) special PHY(+Fiber Optic Transceiver) between MAC (MII) and optic media ;

2) media converter between electrical and optic media.

Note, the LXT971A, mentioned above, supports both standards 100BASE-FX

and 100BASE-TX.

As for media converters, please take a look at the following :  

< http://www.perle.com/products/SFP-Media-Converter.shtml?utm_source=google&utm_medium=cpc&utm_campaig... >

Another (on board chip) approach is as following :

< http://www.digchip.com/datasheets/parts/datasheet/028/AL211-pdf.php >

4,965 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Sergii,

    The following is Mapping of MII signals, and attachment is schematic of a MII PHY named  LAN8700. you can refter to them.

IMX28-MII.png

regards,

Weidong

0 项奖励
回复

4,965 次查看
Radist
Contributor II

Hello Weidong,

thank you for answer!

I forgot to mention, that i am using 100 Base FX SFP, optical module, and it doesn't work with normal PHY.. have tried it with LAN8720...

Do you have expirience with optical modules?

--

Best regards,

Sergii

0 项奖励
回复

4,965 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Sergii,

     Is the PHY you are using is MII 100M ? LAN8720 is RMII, if you want to use MII , you can select LAN8700 or LAN8710 PHY.

regards,

Weidong

0 项奖励
回复