how to connect imx6ulnxpuiopb argon board to wifi and how to configer the gpio?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to connect imx6ulnxpuiopb argon board to wifi and how to configer the gpio?

15,292件の閲覧回数
yashtrivedi
Contributor I

when i connect board using minicom it is booted from the emmc and when i try to modify the wpa_supplicant.conf it says that permission denied even though i work as root usiung 'su' and its also stated that read only file system i even tried to remount it but it says your directory is not in /proc/mnt

imx6ulevk‌ imx6ultralite‌ #imx6ulnxpuiopb#i.mx6 android#androidthings#wpa_supplicant#simple interrupt gpio#gpio-leds

ラベル(5)
1 返信

15,130件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yash

please refer to sect.4.12 Wi-FI BCM4339 attached Linux Manual

for supported wifi modules in nxp official bsps described on

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i....

If other module is used, support may be provided by vendor of used module.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信