how to config gpio interrupt in imx6qsabresd?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to config gpio interrupt in imx6qsabresd?

2,524件の閲覧回数
magicarrow98
Contributor II

Hi, all

i'm used linux 14.04.5 and kernel 3.0.35-4.1.0+yocto+gbdde708.

My board is connected to the GPS PPS signal line and CSI0_DAT6.

I want to generate an interrupt when a signal is received.

what should I do?

menuconfig? board-mx6q_sabresd.c or board-mx6q_sabresd.h edit?

please, Tell me...

Sorry. I can not speak English well. I hope you understand.

タグ(2)
4 返答(返信)

2,207件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jun

one can look at below thread

Proper GPIO interrupt handling in iMX6 

various examples, like configuring touch interrupt can be found in

linux/../mach-mx6/board-mx6q_sabresd.c

Linux-3.0.35_4.1.0

https://www.nxp.com/webapp/Download?colCode=L3.0.35_4.1.0_ER_SOURCE_BSP&appType=license&loca...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,207件の閲覧回数
magicarrow98
Contributor II

Thanks, igor.

But I hope to have a more detailed explanation.

I want to interrupt the signal that occurs once a second, and to count the sysclk between the signals.

I downloaded the package(https://www.nxp.com/webapp/Download?colCode=L3.0.35_4.1.0_ER_SOURCE_BSP&appType=license&loca...) but it did not help. I even had it already.

Is there any other way? I want you to remember that I am a beginner.

0 件の賞賛
返信

2,207件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jun

for beginners suggest to start with linux tutorial:

Linux Device Drivers, Third Edition [LWN.net] 

Best regards
igor

0 件の賞賛
返信

2,207件の閲覧回数
magicarrow98
Contributor II

Hi, igor

I modified the source code to use "CSI0_DAT6" as the GPIO pin.

arm/mach-mx6/board-mx6q_sabresd.h

board_mx6q_sabresd_h.PNG

arm/mach-mx6/board-mx6q_sabresd.c

I added the code.

board_mx6q_sabresd_c1.PNG

Is that right?

If so, what should we do next?

0 件の賞賛
返信