how to config 1PPS on imx8qxp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to config 1PPS on imx8qxp

1,873件の閲覧回数
steven_zhang
Contributor V

i want to hnow which pin is the PPS pin on a imx8qxp processor? the ENET0_REFCLK_125M_25M ALT2? 

how to config it?

0 件の賞賛
返信
1 返信

1,822件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Steven

>which pin is the PPS pin on a imx8qxp processor? the ENET0_REFCLK_125M_25M ALT2? 

yes this is correct. For usage one can refer to sect.4.2 ENET IEEE-1588 i.MX Linux Reference Manual

unit test:

FSL-UT-IEEE1588-001.txt\doc\misc\test - imx-test - i.MX Driver Test Application Software 

https://community.nxp.com/message/1233356 

configuration example

How to add iMX8QXP PAD(GPIO) Wakeup 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信