ERROR: Logfile of failure stored in: /home/fsl-community-bsp/build/tmp/work/cgtqmx6-poky-linux-gnueabi/u-boot-fw-utils/v2013.07+gitAUTOINC+62c175fbb8-r0/temp/log.do_compile.18430
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 2 HOSTCC=arm-poky-linux-gnueabi-gcc -march=armv7-a -mthumb-interwork -mfloat-abi=hard -mfpu=neon -mtune=cortex-a9 --sysroot=/home/fsl-community-bsp/build/tmp/sysroots/cgtqmx6 HOSTSTRIP=true cgtqmx6_config
| make: *** No rule to make target `cgtqmx6_config'. Stop.
| make: *** [cgtqmx6_config] Error 1
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/fsl-community-bsp/build/tmp/work/cgtqmx6-poky-linux-gnueabi/u-boot-fw-utils/v2013.07+gitAUTOINC+62c175fbb8-r0/temp/log.do_compile.18430)
ERROR: Task 6 (/home/fsl-community-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot-fw-utils_2013.07.bb, do_compile) failed with exit code '1'