HI 尚飞 汤
please refer to attached Linux Manual
sect.13.1.1.6 Menu Configuration Options,
13.2 Unit Test, describing how to configure gpu
driver and load/unload it.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear igorpadykov:
thank you so much.
by the way ,can you tell me about how to solve ipu_warning:
<4>[ 1.983397] imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00800000
<4>[ 1.990512] imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00080000
does this warning effected by the ipu/lvds clk settingt?
Hi尚飞 汤
IPU_INT_STAT_10 =0x00080000"
this bit is set as result of data starvation when
data that should be sent to display, but it is not available in IPUs
internal FIFO.
Most probable cause for this issue is huge load on the DDR memory bus.
One can try to decrease bus load: remove unused applications, decrease frame
rate,
bpp (bit per pixel), increase ddr and processor frequency, if possible.
Best regards
igor