how to change the signal mapping pins of 8 bits yuv format for Imx6q?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to change the signal mapping pins of 8 bits yuv format for Imx6q?

ソリューションへジャンプ
3,153件の閲覧回数
MrHoon89
Contributor I

I want to change the signal mapping pins in Table 62. Camera Input Signal Cross Reference, Format, and Bits Per Cycle.

Our hardware is as follows.

MrHoon89_0-1626241110213.png

So, we must use CSI0_DATA[11:4] for 8bits yuv format. 

But, only CSI0_DATA[19:12] should be used in the IPU Sensor Interface Signal Mapping.

MrHoon89_1-1626241284070.png

We must change the pins from CSI0_DATA[19:12] to CSI0_DATA[11:4].

What should i do?

Please help me!

0 件の賞賛
返信
1 解決策
2,686件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
3 返答(返信)
2,738件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the data sheet, for yuv 8bits, connect to the high 8bits

0 件の賞賛
返信
2,735件の閲覧回数
MrHoon89
Contributor I

Do you mean that it is impossible to change the pins from CSI0_DATA[19:12] to CSI0_DATA[11:4]?

0 件の賞賛
返信
2,687件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

yes, I think so

0 件の賞賛
返信