how to change the signal mapping pins of 8 bits yuv format for Imx6q?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how to change the signal mapping pins of 8 bits yuv format for Imx6q?

跳至解决方案
3,043 次查看
MrHoon89
Contributor I

I want to change the signal mapping pins in Table 62. Camera Input Signal Cross Reference, Format, and Bits Per Cycle.

Our hardware is as follows.

MrHoon89_0-1626241110213.png

So, we must use CSI0_DATA[11:4] for 8bits yuv format. 

But, only CSI0_DATA[19:12] should be used in the IPU Sensor Interface Signal Mapping.

MrHoon89_1-1626241284070.png

We must change the pins from CSI0_DATA[19:12] to CSI0_DATA[11:4].

What should i do?

Please help me!

0 项奖励
回复
1 解答
2,576 次查看
joanxie
NXP TechSupport
NXP TechSupport
0 项奖励
回复
3 回复数
2,628 次查看
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the data sheet, for yuv 8bits, connect to the high 8bits

0 项奖励
回复
2,625 次查看
MrHoon89
Contributor I

Do you mean that it is impossible to change the pins from CSI0_DATA[19:12] to CSI0_DATA[11:4]?

0 项奖励
回复
2,577 次查看
joanxie
NXP TechSupport
NXP TechSupport

yes, I think so

0 项奖励
回复