Hi,
we need to change MTU size more than 1500 default on imx8m mini, such as 9000.
I refer to the contents of the two posts to modify my kernel and fec driver, but it does not work.
Solved: Re: How to set jumbo frame? - NXP Community
[PATCH/RFC,net-next] net: fec: allow "mini jumbo" frames - Patchwork (kernel.org)
Although I can set mtu to 9000, but he can't communicate normally.
I have confirmed that the mtu of the target machine has been set to 9000, and can be pinged through with the "-s 9000" parameter.
Regards,
zhouyq