how to can manual ip addresses

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to can manual ip addresses

ソリューションへジャンプ
1,538件の閲覧回数
ebrahimyousufpr
Contributor I

Hi, 

I use imx solox 6 for small network project and i try to use the two ethernet port at the same time for my project, however the first ethernet work successfully(it has IP address ), but for the second ethernet it doesn't has IP address automatically when I connect the cable into the port . how can i give the second ethernet port an IP address manually?

Or is there anther way to fix this problem?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,464件の閲覧回数
b36401
NXP Employee
NXP Employee

You can add the command like "ifconfig eth1 1.2.3.4" into startup script.

元の投稿で解決策を見る

2 返答(返信)
1,465件の閲覧回数
b36401
NXP Employee
NXP Employee

You can add the command like "ifconfig eth1 1.2.3.4" into startup script.

1,464件の閲覧回数
ebrahimyousufpr
Contributor I

thank you very much for your help

0 件の賞賛
返信