Has anyone been able to build an image with gnome-desktop support?
I have been able to build with ltib and the latest downloads from freescale, the version Im able to build does not include any graphical support.
The only graphical image is the one already built.
Any hint is greatly appreciated.
Hello xizhou,
It works fine with new 11.09 BSP ! thank you for your help.
Best Regards,
Philippe Cavenel.
Hello
Build the gnome profile in the new 11.09 BSP for the i.MX53 QSB. It worked fine on the VGA by default with USB mouse support. See attached Log file.
There are differences compare with 1101 BSP.
how to set the clock to 1000Mhz
You log showed the following failure:
Fatal server error:
Segmentation fault caught
matchbox-panel: failed to open displaymatchbox-desktop: unable to open display !
matchbox: can't open display! check your DISPLAY variable.
ts_open: No such file or directory
So please check the settings in /usr/bin/startx is right nor not.
Hello,
My VGA screen is working correctly with UBUNTU on my iMX53 board. But when I build my own kernel with ltib I can't get an image. I just have a root access on serial output. I am trying to get a VGA image with FSL gnome release package profile. I can see penguin image at boot time for some seconds and that's all. Do you know what I have to do to get a desktop environment that works fine ? (setting, packages version, test functions, and so on).
I would like to know also how to set the network to get an IP address ?
Last question, do you know if there is a function such as apt-get or zypper that we can use to install packages on that board with ltib environment ?
Help or link will be appreciate.
Regards,
Philippe.
Hi,
What exactly do you want to do? Gnome is a framework for desktop machines, but MX53 is an embedded system, and most embedded scenarios I know have single application requirements, which are pretty much far away from a full blown gnome or kde desktop.
rsc