how to bootup on ecspi of imx8mq ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to bootup on ecspi of imx8mq ?

2,879 Views
jiangyaqiang
Contributor V

Hi anyone:

         I'm porting android8.1.3 to imx8mq. I success in bootup from emmc, but failed to bootup from ecspi(ecspi1 connected with a nor flash).

         The uboot is the same as the uboot bootup in emmc, and have burn to position of 33K.

         And I have success to boot up with the same "nor flash" in imx6.

         Any suggestion ?

Best Regards.

YaQiang

0 Kudos
Reply
3 Replies

2,611 Views
igorpadykov
NXP Employee
NXP Employee

Hi YaQiang

i.MX8M supports boot from NAND flash, SD/MMC as described in

sect.6.1System Boot i.MX8MDQ Reference Manual (rev.0  1/2018)
https://www.nxp.com/docs/en/reference-manual/IMX8MDQLQRM.pdf

There is no option for boot from ecspi.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,609 Views
jiangyaqiang
Contributor V

HI igor:

In section 6.2.

The boot device can select SPI/nor

江亚强

软件工程师

Shenzhen Huameishi Technology Co., Ltd

深圳市华美视科技有限公司

深圳市南山区科苑路6号科技园工业大厦605

Tel:0755-26037882-616

Mail:yaqiang.jiang@huameishi.com

0 Kudos
Reply

2,609 Views
igorpadykov
NXP Employee
NXP Employee

this is typo, only these 2 modes are supported.

Best regards
igor

0 Kudos
Reply