how to allocate ethernet to linux,   in I.MX8MM-EVK ---in openil1.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to allocate ethernet to linux,   in I.MX8MM-EVK ---in openil1.1

1,135 Views
pengluo
Contributor III

I want to allocate ethernet to linux,  use openil1.1 , in I.MX8MM-EVK ,  we don't use eth0 in baremetal, but linux os use ethernet ,how to do ?  

1. I modify  dts file,  in  output/build/linux-OpenIL-v1.11-linux-imx-202104/arch/arm64/boot/dts/freescale/

imx8mm-evk-revb-baremetal.dts: 

change "disabled"  to "okay"

&fec1 {
status = "okay";
};

2. in  dir/output/build/qoriq-bm-uboot-OpenIL-v1.11-Baremetal-202104$

cancel   [ *] Enable Enable FEC MXC for baremetal   this  Item.

change [*] Enable FEC MXC for baremetal  ----> [] Enable FEC MXC for baremetal

 

result : rebuild  all ,  create   sdcard.img, then burn to  sd

linux os  fail to  boot......

like:

610069 bytes read in 41 ms (14.2 MiB/s)
36217344 bytes read in 1572 ms (22 MiB/s)
Booting from mmc ...
45795 bytes read in 18 ms (2.4 MiB/s)

start  kernel.... ....... 

 

 

make menuconfig

[*] Enable baremetal features │ │
│ │ [*] Enable GPIO for baremetal │ │
│ │ (0) The core GPIO0 assigned │ │
│ │ (0) The core GPIO1 assigned │ │
│ │ (0) The core GPIO2 assigned │ │
│ │ (1) The core GPIO5 assigned │ │
│ │ [ ] Enable I2C for baremetal │ │
│ │ [ ] Enable IRQ for baremetal │ │
│ │ [*] Enable ICC for baremetal │ │
│ │ [ ] Enable QSPI for baremetal │ │
│ │ [ ] Enable FMAN for baremetal │ │
│ │ [ ] Enable USB for baremetal │ │
│ │ [ ] Enable PCIE for baremetal │ │
│ │ [ ] Enable FlexCAN for baremetal │ │
│ │ [ ] Enable ENETC for baremetal │ │
│ │ [ ] Enable SAI for baremetal │ │
│ │ [ ] Enable IFC for baremetal │ │
│ │ [*] Enable FEC MXC for baremetal │ │
│ │ (1) The core FEC MXC assigned

 

nxp document,

4.4.6.4 Ethernet
This section describes the Ethernet configuration settings for .MX8MM-EVK or I.MX8MP-EVK boards.

Disable the ethernet card from dts files:

&fec1 {
status = "disabled";
};

I.MX8MM-EVK has only one NIC, default status of eth0(fec1) is disabled. if user don't use eth0 in baremetal,
can enable fec1 in kernel dts file.

Confirm baremetal configuration

make menuconfig
ARM architecture --->
[*] Enable baremetal
[*] Enable NIC for baremetal
(1) which core that NIC is assigned to

 

0 Kudos
Reply
1 Reply

1,127 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peng

 

one can check enet clock with oscilloscope and configure it using IOMUXC_GPR_GPR1 register

(GPR_ENET1_TX_CLK_SEL) described in sect.8.2.4.2 General Purpose Register 1 (IOMUXC_GPR_GPR1) i.MX 8M Mini Applications Processor Reference Manual

 

Best regards
igor

0 Kudos
Reply