how to add bluetooth in imx6q_sabresd?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to add bluetooth in imx6q_sabresd?

Jump to solution
2,856 Views
weisheng
Contributor III

     hello,I have a imx6q_sabresd board,but there are just a bluetooth slot,what type of the bluetooth device should  I bought? Is the android-4.4.3 support bluetooth by default?if no,what should i do to make it support bluetooth?

     I am a newer,please help ,thank you!

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
2,121 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi weisheng,

In our Android_Release_Notes.pdf  you can see that the default board support the follow :

Connectivity - BT

Hardware:

• Silex AR6233X SDIO card

And there are some useful threads you can refer to:

How to enable BT on board imx6q_sabresd RevC.

All Boards Bluetooth Dongle

USB Bluetooth Dongle not working

Hope this can help you.


Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,122 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi weisheng,

In our Android_Release_Notes.pdf  you can see that the default board support the follow :

Connectivity - BT

Hardware:

• Silex AR6233X SDIO card

And there are some useful threads you can refer to:

How to enable BT on board imx6q_sabresd RevC.

All Boards Bluetooth Dongle

USB Bluetooth Dongle not working

Hope this can help you.


Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,120 Views
weisheng
Contributor III

hi dan wang,

thanks for fast reply,your answer help me a lot,i am trying.

0 Kudos
Reply