how osd work on imx6q?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how osd work on imx6q?

ソリューションへジャンプ
2,807件の閲覧回数
stevenhuang
Contributor III

I wan the video as the input of fb0, QT frame as the input of fb1; video is background, QT  picture is front, but no QT picture been display.  Where can i find document about this issue?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,502件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 友 杨 

please check below links which may help

IPUv3 frame buffer question (./driver/video/mxc/mxc_ipuv3_fb.c) 

i.MX6: fb2 Framebuffer issue 

A Deep Dive into Image Processing for i.MX 6 Series Applications Processors 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

4 返答(返信)
2,502件の閲覧回数
yyuan
Contributor III

hello

please  do you solve the peoblem?

i have the same problem.

please help me

thank you

0 件の賞賛
返信
2,502件の閲覧回数
stevenhuang
Contributor III

I  am sorry,  the FB0 is FG, fb1 is BG. but i fond the BG have no any picture display.

0 件の賞賛
返信
2,503件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 友 杨 

please check below links which may help

IPUv3 frame buffer question (./driver/video/mxc/mxc_ipuv3_fb.c) 

i.MX6: fb2 Framebuffer issue 

A Deep Dive into Image Processing for i.MX 6 Series Applications Processors 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,502件の閲覧回数
stevenhuang
Contributor III

thank you,  i have fixed my issue: the alpha value is 0 by default, so the BG can't display.

0 件の賞賛
返信