how many trustzone tech used in i.MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how many trustzone tech used in i.MX6DL

1,745 Views
qingxiangluo
Contributor I

Refer to the user's manual of i.MX6DL:

Document Number: IMX6SDLRM

Rev. 1, 04/2013

and just find some words for trustzone, so i want to know how many TZ IP/tech is used in i.MX6DL?

like TZPC,TZASC? or whether NXP has special document for trustzone related topics?

in the bootloader, whether it already support trustzone feature?

thanks!

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,433 Views
igorpadykov
NXP Employee
NXP Employee

Hi qingxiang

security features are described in Security Manual attached on

Q&A: How is mx6 PMIC_ON_REQ under SW control? | NXP Community

secure boot on application note AN4581

http://www.nxp.com/files/32bit/doc/app_note/AN4581.pdf

for TrustZone one can use arm resources:

TrustZone - ARM

https://www.sbs.ox.ac.uk/cybersecurity-capacity/system/files/ARM%20Security%20Technology.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,434 Views
qingxiangluo
Contributor I

Hello igor,

          To use TZ technology, is it possible to separate GPU 2D/3D to different world? like 2D for secure while 3D for Non-secure?

how?

0 Kudos
Reply