how easy is it to change the UART 4 (M7 Debug) for user Appliktion on MIMX8MN6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how easy is it to change the UART 4 (M7 Debug) for user Appliktion on MIMX8MN6

Jump to solution
1,744 Views
Sal2020
Contributor II

Hi,

Is it possible to use UART4 for other application (Not for M7 debug) without hardware changes on i.MX8M Nano?

Can I change the UART 4 for other device communication only via Software like (u-boot, Linux and systemd)?

 

I don't want to change UART4 as A53 debug like here I would like to stay UART 2 for A53 debug.

 

regards

 

0 Kudos
Reply
1 Solution
1,733 Views
igorpadykov
NXP Employee
NXP Employee
2 Replies
1,708 Views
BiyongSUN
NXP Employee
NXP Employee

The document tells you everything. Your case is just the subset in the document. 

0 Kudos
Reply
1,734 Views
igorpadykov
NXP Employee
NXP Employee

Hi Saleem 

 

one can look at dts example with uart4

https://github.com/digi-embedded/linux/blob/v5.4/dey-3.0/maint/arch/arm64/boot/dts/digi/ccimx8mn-dvk...

 

Best regards
igor