how easy is it to change the UART 4 (M7 Debug) for user Appliktion on MIMX8MN6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how easy is it to change the UART 4 (M7 Debug) for user Appliktion on MIMX8MN6

ソリューションへジャンプ
1,908件の閲覧回数
Sal2020
Contributor II

Hi,

Is it possible to use UART4 for other application (Not for M7 debug) without hardware changes on i.MX8M Nano?

Can I change the UART 4 for other device communication only via Software like (u-boot, Linux and systemd)?

 

I don't want to change UART4 as A53 debug like here I would like to stay UART 2 for A53 debug.

 

regards

 

0 件の賞賛
返信
1 解決策
1,897件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
2 返答(返信)
1,872件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

The document tells you everything. Your case is just the subset in the document. 

0 件の賞賛
返信
1,898件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Saleem 

 

one can look at dts example with uart4

https://github.com/digi-embedded/linux/blob/v5.4/dey-3.0/maint/arch/arm64/boot/dts/digi/ccimx8mn-dvk...

 

Best regards
igor