how do I recover from sda stuck with a bare metal imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how do I recover from sda stuck with a bare metal imx6

752件の閲覧回数
rogergipson
Contributor I

Please help, If anyone knows the answer.

I am having a devil of a time with sda being stuck during reads on the i2c bus for a single core imx6.

I NEED bare metal code for the i2c routines for the imx6 .. I am very far behind now.  Any help would be appreciated.

Thank you...

Tecfacet at yahoo dot com

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

596件の閲覧回数
YixingKong
Senior Contributor IV

Roger, please click Corret Answer/Helpful answer, if your question has been answed.

Thanks,

Yixing

0 件の賞賛
返信

596件の閲覧回数
israelpz
Senior Contributor I

Hi,

The SDK have bare metal driver for i2c and also a a test example.

You could get it in the i.mx6 download page only select your desired processor (i.mx6q or i.mx6dl, etc).

For example the i.mx6q is in i.MX6Q Product Summary Page is under Snippets, Boot Code, Headers, Monitors, etc. (3).


Check under sdk/drivers/i2c. The i2c code depends of other code like pll.


Regards,

-Israel.

0 件の賞賛
返信