how do I configure the i2c host with clock stretching ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how do I configure the i2c host with clock stretching ?

ソリューションへジャンプ
3,636件の閲覧回数
Luke-Hsieh
Contributor III

I'm trying to have TI gauge bq27542-g1 worked on imx8m nano EVK with pure Linux OS.

I was aware that i2c host must support i2c clock stretching to wait for slow slave response.

 

Can anyone share your experience any specific change in DTS or in the driver to support i2c clock stretching ?

 

 

ラベル(3)
0 件の賞賛
返信
1 解決策
3,624件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Luke

 

it is supported in hardware as described in sect.15.1.3.5 Clock stretching, no additional

dts settings are needed   i.MX 8M Nano Applications Processor Reference Manual

 

Best regards
igor

元の投稿で解決策を見る

2 返答(返信)
3,613件の閲覧回数
Luke-Hsieh
Contributor III

Hi Igor,

 

Thanks for the confirmation!

I will give it a try when I receive the device which is a fuel gauge IC.

0 件の賞賛
返信
3,625件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Luke

 

it is supported in hardware as described in sect.15.1.3.5 Clock stretching, no additional

dts settings are needed   i.MX 8M Nano Applications Processor Reference Manual

 

Best regards
igor