how can we capture raw-PCM 6 channel audio from imx-6 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how can we capture raw-PCM 6 channel audio from imx-6 ?

1,398 Views
nagendrasarma
Contributor III

hi Freescale,

how can we capture raw-PCM 6 channel audio from imx-6 ?

we do not even want ALSA

regards

Nagendra

0 Kudos
Reply
3 Replies

1,171 Views
igorpadykov
NXP Employee
NXP Employee

Hi nagendra

yes, up to 32 time slots (channels) are supported in SSI Network Mode,

IMX6DQRM sect.61.8.1.2.2 Network Mode Receive

Figure 61-15. Network Mode Timing

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,171 Views
nagendrasarma
Contributor III

thank you igor,

that should be fine, could you please share any test apps/driver  to achieve the same , you can even suggest the link/sdk info etc.

regards,

Nagendra

0 Kudos
Reply

1,171 Views
igorpadykov
NXP Employee
NXP Employee

Hi nagendra

I do not know such example, suggest to reuse ssi example from SDK

"MX6_PLATFORM_SDK "

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeId=018rH3ZrDRB24A&fpsp=1&t...

~igor

0 Kudos
Reply