i want to know how to use imx233 for linux ,such as how can i download bootloader to the chip,i had read many document about imx233,but i can not find the answer.
Hi steven,
Our expert have given you the link of BSP and tool for i.mx233. You can refer to i.MX23_Linux_BSP_UserGuide.pdf and use the mfgtool Mfgtools-Rel-1.6.2.048 to download.
Have a nice day
Dan
Please refer to the documentation for the L2.6.31 Linux BSP for the i.MX233 EVK
board by FSL/NXP, available on the i.MX233 Documentation web page (check the
"Supporting Information" section):
The BSP itself can be found on the i.MX233 Software&Tools
web page (check the "Board Support Packages" section):
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,Artur,
thanks your answer,it is great!
if i can download bootloader by usb,i do not need the sjtag,is right?
Hi,Artur,
I have not fine the reset pin of imx233,and i want to confirm that the reset key is used to cut off the supply power and put the XTALIN pin to gnd int imx233 evk sch,is right ?
Yes, your understanding is correct. i.MX233 doesn't have its own Reset input, so, the Reset signal of the system just stops the 24MHz XTAL oscillation and cuts the 5V power to emulate the power cycling of the processor.
Best Regards,
Artur
Hi Artur
You are great!
where i can download the datasheet of LCD module in the imx23 EVK,i want to learn how to use LCD interface.
Hi,Artur
Where can i find the attach,i am so sorry i can find it in the community.
Do you mind i can find it in the evk schematic? may be it is difficult to me ,can you give me some reference how to use the LCD interface?