how can i use can bus with mx8 family processor ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how can i use can bus with mx8 family processor ?

1,162件の閲覧回数
dogancanyuksel_
Contributor I

i did not find in datasheet ? i need harware can bus but also i can use software part.

Is mx8 quad core processor has bus protocol is not it?

ラベル(1)
0 件の賞賛
返信
1 返信

1,093件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi dogancan

yes i.MX8QM has can module, one can look in linux documentation and try unit tests

Alpha / Beta BSPs for Microprocessors|NXP 

doc\can\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信